Hallo all,
I have got a Problem with the activating the CW-mode of the DW1000.
I want to check und trim the frequency of the oscillator from the EVB1000.
The „DW1000 USER MANUAL“ (capital 8.1 “IC Calibration – Crystal Oscillator Trim“) says I have to write at the “Sub-Register 0x2A:0C – TC_PGTEST“ a 0x13. Now the CW-mode should be activated but the spectrum analyzer didn’t show any change and at the “[size=medium]0x0F – System Event Status Register” are all bit set.
The same happens when I use the function “[/size]dwt_configcwmode“ from the “DW1000 DEVICE DRIVER APPLICATION PROGRAMMING INTERFACE (API) GUIDE“.
Is this correct what is shown at the status register?
How I able to recognize the variance of the oscillator frequency on the spectrum analyzer?
Best regards
Zennekk