Hello everyone,
I’m working on a setup with several DWM3001CDKs. In this setup, one device acts as a controller that collects distance measurements from the controllees. Based on certain conditions, the controller should also be able to send a custom notification to one of the controllees.
The provided examples (e.g. TWR, or a device configured as RX with another as periodic TX using a custom PSDU) work correctly. However, I haven’t found a way to:
- integrate custom PSDUs into the TWR example, or
- implement a complete transceiver mode with custom messages.
My questions are:
-
Is it possible to implement this kind of setup using FiRa or UCI? I noticed in the documentation that section 5.8 states “[Not supported in QM33 SDK] Sending data over a FiRa session.”
-
If not, is the right approach to write my own stack using the
uwbmac.hfunctions? Are there any minimal TX/RX examples available? TheHelloWorldexample only prints device info and doesn’t demonstrate TX or RX handlers.
Best regards,