Since the firmware that came with the DWM1001-DEV does not fit my needs, I need to write my own for the DWM1001 with custom messaging.
I have no prior knowledge of the DW1000 or DWM1000, but just downloaded the DW1000 API rev2 and looked through some examples.
Is it possible to transfer these to the DWM1001(-DEV)? I see some custom code blocks like “peripherals_init”, which obviously need to be rewritten for the NRF52, but is there any major issue that prevents me from doing so?
Before I start digging deeper I just want to know if it’s worth it
Yes, Decawave plan to post a stand-alone Keil MDK project with TWI/Accelerometer/UART configured.
In addition an Initiator/Responder example from the DW1000 API examples.
Expect this to be delivered in the coming days.
Was this ever done?
I am interested in using DWM1001 hardware with the old deca-api stack already built into it to enable fast development (and simple processor porting for my host applications) of Initiator/response apps like the SSR.
ie. It would have all the dwt_devid, dwt_Reset() etc commands that I could call via the SPI from external processor.