Cross reference for Agilent ABA-52563-BLKG

Hi

I am looking for a replacement for a Agilent/Broadcom chip, and I was thinking that Qorvo should have that.

Here is a link to the chip that is obsolite:

For our application, we are only interested in the performance between 10MHz and 500MHz. The noise figure should be below 1.1dB and the gain above 20dB. The supply voltage between 3 and 5 Volt single supply.

If you need something in the same package then the AG203-63G or AG303-63G are closest. Note slight difference on pin 4 usage.