Hello,
Is there any way to use host other than Raspberry pi for communicating with bridge node?
Thanks
Asmita
Hello,
Is there any way to use host other than Raspberry pi for communicating with bridge node?
Thanks
Asmita
Hi Asmita,
At the moment only the raspberry pi 3b is supported.
Yves
Hi Yves,
Is there any way in which I can know what TLV commands are being sent between Raspberrypi and the bridge node?
Thanks & Regards
Asmita
Hi Asmita,
The interface is not documented at the moment so I don’t think it is possible.
Thanks
Yves
Hello Yves,
Thanks for your response. I tried to obtain that using logic analyzer by reading the SPI transfer between rpi and the bridge. I obtain the result as attached in the csv file.
I have two tags i.e DW5B37 and DW9B31 each of them is sending iot data to bridge in while loop. One tag is sending IoT data as “Lzerowav” and other tag is sending “LFountlab”. In the data obtained using logic analyzer , I can see these “LFountlab” and “LZerowav” data.
But still there are lot of confusion I am having right now.
Because as per the document, SPI is half duplex when either master or slave sends the data, the other should send dummy data as 0xFF but here i find that both side are sending data together.
Kindly look at the attached link and suggest if you can infer from it anything.
Thanks & Regards
Asmitahttps://drive.google.com/file/d/16xn_4oXfDtPaA-_KFcOyVCo_2VaNdNXR/view?usp=sharing