Hi,
I’m triyng configure a bridge, but some problems are dificult this task.
I flash the DWM1001_PANS_R2.0.hex in the DWM1001-DEV’s boards and using the balenaEtcher. I flash the raspbian image into raspberry pi 3 model b v1.2.
bridge config:
anchor 1:
anchor 2:
anchor 3:
anchor4:
I try connect with the raspberry via ssh but I can not. I think it’s strange the green led of raspberry only flashes 3 times, and the light of network cable does not turn on.
Raspberi pi:
to check if the problem is not raspberry I try with a raspbian imagen on the raspberrypi.org and with this image I connect with the raspberry via ssh and the green leds works well.
Hello CostaT !
I couldn’t raise raspi until I burn the image on a 32 GB card. With smaller cards it simply did not start, maybe you have similar problem
end kernel panic-not syncing:VFS: unable to mount root fs on unknow-block(179,2)
will be the size of the card??
The NOOB image works and the balenaetcher also works with boyh images.