I am using qorvo QM33120WEVB . I have total of two devices which means i can have one initiator and 3 responders. I am using currently use two of them.
i can only get response from one device .
Can someone suggest what configuration to use for this kind of system
Hi @shashank
it should work normally. Do you always get response from only one device (no matter if it is single antenna / PDOA antenna device)? The PDOA device has a directional antenna so must be faced always to the PDOA initiator.
Cheers
JK
I get response from one device only . The device configuration doesn’t matter.
Hi @shashank
I have rechecked and the current version support only one device. But in future it should support multiple devices.
Cheers
JK
Hello, quick question.
Did set up anything when connecting the board to the gui? Or did you simply just plugged them in the laptop with an usb?
I am struggling because in the guide book it says that the board is preprogrammed and just plugging in will be enough. However I am not seeing any devices in the GUI. If would be very kind of you to offer some help 
Does it support multi device now? Also, I only get response from one device, even if configuration doesn’t matter.