How many concurrent connection (communication) is supported by the Gateway? i. e. If the Gateway has hundreds of tags (assets), how many can it communicate with simultaneously? How can it manage tags if the max number is reached?
Does the Gateway manage the assets and the asset requires logic (make and break connection) to communicate with the Gateway?
Hi Arun,
Per the current implementation. the gateway supports 140Hz on tags location (so effectively full capacity).
For uplink and downlink data it is a bit more complex and I can’t quite answer yet as we may modify the architecture in the near future.
The gateway is listening to the network and transmitting at determined slot during which assets will listen to it. There is no logic control between assets and gateway.
Thank you,
Regards
Yves