Hey All,
I am having an issue where two different listeners are not able to communicate among themselves.
I have a setup where I have 5 anchors in a room and 2 tags. Moreover I have two tags setup as listeners. Total 9 hardware.
Now I have rasp 3b connected to both the listeners. I can see the data of two tags in the terminal through both the listeners. Now if I take listener-1 out of the range of tags, but in the range of the listener-2 (at this time, listener-2 is still getting data of the listener), am not getting any data in listener-1.
Is there any way through which I can data from one listener to another?
Use case : Let’s say I have an area of 2000 sq m, and I have listeners at regular interval, how can I get location of one tag which is at another end with the listener which is equipped with rasp on another end.
Thanks.