Hi!
I’ve been working with dwm1001 for a while. And have got several cases which usually happens. Maybe you can help me.
Case 1 (tag is not seen by a listener)
- I have a system with PANid = 0002 in my office.

- I’ve got tag (333c) and changed it PANid from 0001 to 0002

- I checked if it could see any anchors

It could.
5. I have done several resets and several factory resets, but it still is not visible for my listener. It’s seen by my phone. What can I do?
6. Listener settings.

CASE 2 (many problems with dwm)
- I have mdek module (147b). It has been working for a long time (1 month).
- Once I couldn’t connect to it by means of any interfaces and it like disappeared. Than sth happened to firmware. It has got id 0000; it couldn’t work and be defined by listener.
- After a while it repaired (somehow) and returned to it previous working state.
- I turned it off yesterday.
- Today I wanted to check it. It’s defined as COM port but Enter/double enters didn’t work. I turned it off again.
- I turned it on after 30 minutes. Now it’s answering me. But it still can’t be seen by Listener.


- What is the problem? Why has it happened and why listener doesn’t see it.
CASE 3 (dwm1001 are seen only after rebooting a listener)
- Everything became well after I made listener Reboot.

- Should I Reboot listener every time If I want to see a tag? Looks like not normal thing.
CASE 4 (not answerind via COM) - I connect to device. Com port is defined. But I Cannot connect to it (speed is 115200).
- After a while/many tries it’s connected and can be configured.
- It’s a common situation. What should I do to decrease an amount of this situations?
CASE 5 (BLE problems)
- I have 6 devices. All of them have ble on. But 1 of them can’t be seen by my phone
- I start to configure the system using phone. Another device becomes invisible for me
- I connect to it via TeraTerm. It can’t be connected
- Atfer a while/many tries it’s connected. I make factory reset.
- Everything is fine.
- Why did it crash while I was configuring it via BLE?