Hello all,
I just bought a DWM1001 unit, previously I already had MDEK1001.
can I program/FLASH the new DWM1001 by connecting the wire to the junction that is available on MDEK1001??
what I think is:
-
unsolder the following junction:
(J18: SWCLK),
(J17: SWDIO),
(J5: LEDs ??),
(J3: 3V4)
-
Connect the pins of new DWM1001 (single unit) to T … which is in the back part of MDEK1001:
(TP3: 3V4_Segger),
(TP4: SWDIO_OB),
(TP5: #RESET_OB),
(TP6: SWCLK_OB),
(TP7: GND)
I previously read that I could program the DWM1001 using J-Link BASE, because the DWM1001 is NRF-based …,J-Link BASE Classic (8.08.00) - SEGGER U.S. Web Shop
but I don’t have this tool and if I buy it takes time and money,
thank you in advance,
Best Wishes.
Do you really want to do that? The DWM1001-DEV, what you are showing in the picture, has a J-Link On board!
Just plug into the USB port and on your PC you will be able to use J-Flash tool to program. J-Flash comes with the Segger J-Link pacakge avaialbe for free from the Segger.com website. So n need for a separate J-Link BASE or otherwise.
1 Like
oh sorry for misunderstanding Mr.Kenneth.
The MDEK1001 what I mean is DWM1001-DEV, I just open it up then this is how the inside looks like
the thing that I want to FLASH/Program is the single unit of DWM1001 Module, like this:
I have two single unit of DWM1001, and I have one MDEK1001(/DWM1001-DEV), But I don’t have portable J-Link
that’s why I thought that I could program a single unit of DWM1001 using DWM1001-DEV which already has J-Link on board - but I’m not sure how to do it 
Yes, it is of course possible!
there is a thread or two on this
Eg: Mininum pins to enable DWM1001