When the tag’s responsive mode is turned off, there is an error of about 5 meters from the actual position.
Then when the responsive mode is turned on, it returns to the actual position.
after, If I turn off responsive mode again, tags return to the error position in 5meters.
Is this a normal reaction?
no, that is not an expected behaviour. Can you please provide details about your installation? (how many Anchors, position of Anchors, how many Tags, what is the configuration of the Tags, …).
Please send also example output of the ‘les’ command for the Tag in Responsive and Low Power mode.
do the position of the tag in responsive mode ON correspond to the real position? I cannot find the real position in the image you sent.
Could you please send the output of the les command in the Responsive ON and OFF mode?
It might help us to identify the issue. Please send also output of the stg command.