Hi,
We are using the following configuration.
Channel - 5
PRF - 16Mhz
Preamble Length - 128
PAC Size - 8
Preamble code - 3
Use non-standard SFD - false
Data rate - 6.8Mbps
Standard PHR Mode
We are sending 69 bytes of data in continous frame mode for power calibration.
We have used Decawave power calculator tool for calculating the frame duration. Total frame duration as per the calculator is 239.74µs. So if we change the BOOSTP250 value power should get changed. But in this case, there is no variation in power by changing BOOSTP250 values. But what we have noticed is, power is getting changed by varying BOOSTP500 register value. Also if I change the frame size to 65 bytes(235µs) power is getting changed by varying BOOSTP250 register.
What could be the issue???
Regards,
Shijo Thomas