I have a buck converter that is working excellent in the time domain as noted by its output regulation and performance when performing a load step test. However, when I perform a Bode plot test, the frequency response is rather odd to say the least.
You can plot transient results during .bode analysis, which helps with troubleshooting.
Here, I removed the “;” before debug to enable debugging (plotting .tran results during .bode) and also added the FB net name. Now, you can see that everything goes wrong at 20ms (19.5ms in the graph + 500us in .bode Tsettle), which occurs because you still have a pulsing setpoint. Change the pulse source to a constant 0.7V and the problem will be resolved.
I actually do have a constant load for bode plot testing. The step response is performed only during the transient load step response. If you’ll notice, I have the switch and load resistor as “Do Not Stuff” in the Load Step section of the circuit.
Ok, yes, I see where I went wrong. I had forgotten about the Vref source being constant. I thought that by removing the prolonged rise time (i.e., soft-start) would be enough but apparently not the case.