Hello, I am using DWM1001 modules to read distances between tag-anchor. I have 1 tag and 4 anchor, I made an script in python that I run on the terminal of my raspberry pi and get the distances between the tag and the anchors but I only receive 20bytes so I can´t get the full information. I know that I have to change MTU to read/write more than 20 bytes but I don´t know exactly how to do it, can any body help me?
Thanks.
Hi @laura.ece !
I’ve never tried what you’re doing, but I have a suggestion.
I believe the BLE app configures the MTU size before starting communication.
Using an RPi you may try bluez:
$ sudo apt install bluez
Then connect to the device and set the mtu size using the following commands:
$ gatttool -b <mac_address> -I
mtu <size>
After sending the command, the device should respond with a confirmation message. Then you can exit the gatttool by typing exit (or pressing Ctrl+C).
Once you have set the MTU size, you should be able to read/write more than 20 bytes of data from the remote device.
Let me know if it worked!
Best regards!
I have bluez version 5.47, this is the response I got:
pi@raspberrypi:~ $ gatttool -b dd:09:56:ee:61:8a -I
[dd:09:56:ee:61:8a][LE]> mtu 150
Command Failed: Disconnected
[dd:09:56:ee:61:8a][LE]>
Hi, @laura.ece !
One more thing is, the BLE device must support a larger MTU size, and I don’t know if 150 bytes is ok for a DWM1001 module. If you’re not sure, you can try a small value and see if it takes effect.
By the way, which python BLE library are you using? It probably has a function to set the MTU size inside your script.
Best regards!
Hello, I have tried with mtu 30 and it´s still the same error. The librarys I´m using in python are:
import os
import sys
import pygatt
import time
import logging
import binascii
from binascii import hexlify
import struct
import subprocess
Thanks.
Hi @laura.ece!
Using pygatt you can try to set the MTU size right after connecting using .exchange_mtu(size):
adapter = pygatt.GATTToolBackend()
adapter.start()
peripheral = adapter.connect(mac_address)
# Set the MTU size
peripheral.exchange_mtu(size)
Best regards!