Hello,
I’m using a DWM1001-DEV.
After I replace the STM32F072CBT6, It doesn’t work anymore to re-flash and communicate.
Can anyone share me the .bin file that runs on it?
Thanks in advance
Hello,
I’m using a DWM1001-DEV.
After I replace the STM32F072CBT6, It doesn’t work anymore to re-flash and communicate.
Can anyone share me the .bin file that runs on it?
Thanks in advance
You have erased the JLINK-OB firmware. Segger license terms do not allow us to distribute the firmware.
I got it. So, how can i do?
Is there any good way?
I am afraid not. You have ‘bricked’ the unit.
If you have a JLINK or other SWD Debugger, you may be able to hot wire that up.
@Jea,
Maybe I can help you.
I flashed the DWM1001 using an Segger J-link Edu with the Pin SWD on the DWM1001.
SWDIO → PIN3
SWCLK → PIN2
RESET → PIN33
Be sure to disconnect the STM32 with unsolder the correct jumper.
If you want i can take a a photo of the assembly.
@DavidF
can u share the photo?
Thank you so much.
Hi @Jea,
Yes, when I took the photo one little wire just desolder from the board.
Look at the Segger EDU datasheet for the correct pin. Just as a reminder you will need :
You will need to power the the DWM1001_Dev with the USB, or you can active a configuration in the Segger EDU to power up the DWM1001_DEV.
I hope that will help you.
@DavidF
Ok, I’ll try it. Thank you so much:)
No problem.
Also I mention it above but you need to desolder the jumper : J16 - J12 - J6 at the top of the DWM1001