Hi All, Im looking for some advice for a unique situation, a little different to the regular tracking within a room full of anchors.
In short I want to create a base station that will form my anchor. The tag would move around this anchor and I would be able to track both distance and position of the tag. The tag would operate within 5-10m of the anchor and accuracy needs to be accurate to around 0.25 - 0.5m. Both the tag and base station have a BT BLE link for other functions.
The base station ideally would be about 300mm diameter and include x1 UWB module with x3 Antenna. (trying to keep cost to a minimum and avoid the use of multiple modules).
My question apart from the feasibility of the above is what is a the best method to use for tracking and what type of hardware is recommended for the base station.
For efficiency i would like to use PDoA so the tag is sending blinks at regular intervals. These are received by the x3 antenna presumably at different times and location is determined.
I am struggling to understand how the distance is then determined?
It is not feasible to add a clock to each device to synchronise timestamps but i could start a clock on the anchor & tag at the same time (initiated by the BLE from the tag) assuming there would be some error between the clocks (but this would be minimal over the operating distance?).
I have looked at TOF and TDoA but assume these will require more than x1 module in the base station?
I may be overcomplicating this but its been hard to find any examples of tracking a device like this.
As always, appreciate any help/explanation.