A native version would be perfect, but also a version that runs in Wine would be very helpful.
When I try to install QSPICE in Wine, I get the error message
QSPICE requires Windows 11 or a 64 bit edition of Windows 10.
although I use Wine in “Windows 11” mode by selecting this Windows version in winecfg. The same message appears when I try to run QUX.exe (copied from a Windows installation) in Wine. Both, QSPICE64.exe and QSPICE80.exe seem to work well in Wine, but I’d be happy to be able to use the excellent schematic capture and plot tool of QSPICE as well.
Great question! QSPICE uses the GPU (either CPU-integrated or discrete) for both dithering the schematic and plotting the waveforms. The waveform plotting benefits dramatically from the GPU since it means no data compression is required, and yet the waveforms render extremely quickly. We’ve been testing QSPICE under WINE and have run into a number of challenges related to GPU support. It’s a topic we want to address in the future. We understand the interest in Linux support. For now, command-line support under WINE is possible, as you’ve noted, so we hope you can take advantage of the advances the QSPICE simulation engine brings.
We’d love to, but the user interface is designed around GPU acceleration. We’ll continue to monitor Wine’s progress, and Wine support will stay on our radar.
has there been any update on this? There have been many advances in WINE wrt GPU acceleration, particularly in the fork proton (maintained by valve). Would be cool to know if this was revisited or any progress was made. if not, I’ll give it a shot myself at some point. Would you be so kind to let us know which runner and options you use with your WINE command line?
I’ll add that I’ve been using it recently a lot and it runs great under the normal system Wine. And it even runs better if you are willing to run the less stable wine-staging version; but this requires that you displace the stable Wine on your system if you don’t want to use a separate environment or jump through other hoops.