Hi I am using DWM3001cdk and DWM3000 with nrf52840 for UWB
The qorvo Nearby interaction Application introduced through that product page are NIAccessory([1]) and the version of a patch([2]). // Qorvo_Apple_Nearby_Interaction_Beta_release
Where can I get source codes(maybe swift) âNearby interaction Application which exist in Appstore[3]â?
It is far nicer than the apps above([1][2]).
Then with the similarity of names and comparability of codes used in DWM3001CDK for [1], I thought the apps (of [3] and [4]) are an upgraded version.
But are codes of App [3] and [4] private?
Could I get source code( maybe SES project and swift) about âQorvo NI Background Appâ[4] which is in Appstore?
This app didnât find My DWM devices which were founded and connected to other apps[1][2][3].
The part can be skipped below.
At first, I wanted to use DWM 3001cdks.
However, the software that fit right in was small except for several examples, and many software provided in âDWM3000 API Software and API Guideâ didnât work.
(I try to do. But it took so many times cuz itâs my first time )
Because there are few application available and fitted right in DWM3001cdk, I wanted to get the source code of [3][4]. I think Nearby interaction application is only a powerful App.
Now, my period of development doesnât remain a lot.
I wonder if I just donât find materials about the app of [3] and [4]
The sources for both, iOS and device are part of a new release that will be available on Qorvo website anytime soon.
The Background app uses a new BLE service and will not find your device, youâll have to update your devices with the new firmware, when available.
Iâll ping here again if I have any news!
Kind regards!
Qorvo Nearby Interaction Software package v.3.0 is finally here, including sources, binaries, and documentation (embedded firmware, example application, mobile application)