It is useful for automotive application, such as ISO16750 and ISO7637 pulse.
LTspice and Simetrix both support.
It is useful for automotive application, such as ISO16750 and ISO7637 pulse.
LTspice and Simetrix both support.
Yes, you can put ISO16750 and ISO7637 waveforms in QSPICE without resorting to playing a PWL from a file into the simulator.
I’ve forgotten the spec’s, but this should show you the idea.
I think the meanings of the EXP parameters are somewhat non-standard. I didn’t like that TD2 was based from the start instead of the last thing that happened like in a PULSE source.
–Mike