Is there any tutorial or guide how can I read position data in Arduino?
If I have 2 DWM1001-DEV board, how can read two way range data from an Arduino board? How can I connect a DWM1001-DEV to an Arduino is there any diagram? Is there any sample code?
Currently we do not have an Arduino code example. There is a code examples for Raspberry Pi that could be adapted to your needs. Also the data is available via UART or SPI.
Thanks for your reply,
From the datasheet I can only find a raspberry pi sample.
If I understand it correctly, DWM1001 PIN18 is UART RX and PIN20 is UART TX so I should connect those 2 pins to my Arduino board?
From the firmware user guide there is only a sample for raspberry pi, is there an Arduino library I can use?