KSKelvin. The high output level is formed by Darlington. That is, the output level is not equal to the supply voltage, unlike CMOS timers. I suggest a small upgrade of the model.
NE555_comp.qsch (13.7 KB)
KSKelvin. The high output level is formed by Darlington. That is, the output level is not equal to the supply voltage, unlike CMOS timers. I suggest a small upgrade of the model.
@bordodynov Is this the change you recommended in the model? Is there anything I may have missed? The model I developed is generally closer to a device in a textbook rather than being match to the datasheet, which is why there may be room for improvement.
B3 Out COM V=if(V(Q)>0.5,V(Vcc)-0.9,0) Rser=30
You recommend Rser=30 or =40? The netlist in .qsch is 30 but comment is 40.
I was looking for a compromise value and settled on 30 ohms. Have you noticed how your model does not correctly calculate the current of the load capacitor? The resistor improves the situation.
My symbol library has been updated. Rout and headroom voltage are implemented as instance parameters, allowing users to adjust them based on the physical conditions. Additionally, a new symbol with an internal circuit drawing (555Timer-4.qsym) has been created, and the width of the box of -1/-2/-3 has been adjusted to better match with your 555 timer.
Also updated NE555 in qspice-alternative directory, which contains alternative symbols for the built-in NE555 in Qspice.
Oh, thank you for your review and suggestions! Upon checking the datasheet, I realized that the headroom can be up to 1.7V. After comparing it with your symbol, I found that it better matches at a headroom of 1.2V. I also updated the output B-source with IC=0 to ensure it does not output voltage in the DC operation point calculation.
NE555_comp.qsch (9.5 KB)