Alternate Version of Monte Carlo Schematic Capture

There were some LinkedIn questions on the Monte Carlo schematic capture (QSPICE Schematic Capture #070). Here’s another version of that circuit. Active_filter_Monte_Carlo2.pfg (212 Bytes)
Active_filter_Monte_Carlo2.qsch (12.3 KB)

1 Like

Thank you @mccunets ,

I’d like to note two potential issues with QSpice with this sim.

Issue #1:
If you execute the sim, you will get the same EXACT GC() values for each step every time you run it. This is an issue if you’re trying to get a good random sample of the monte carlo.
Here’s a partial output captured of the “random” avol1, gbw1, avol2, and gbw2 parameters for the 1st run and the 2nd run.

step avol1 (run 1) avol1 (run 2) gbw1 (run 1) gbw1 (run 2) avol2 (run 1) avol2 (run 2) gbw2 (run 1) gbw2 (run 2)
0 200000 200000 4000000 4000000 200000 200000 4000000 4000000
1 302984 302984 3708310 3708310 217799 217799 4270940 4270940
2 222748 222748 4398300 4398300 182279 182279 3958960 3958960
3 234451 234451 4380060 4380060 190246 190246 4552230 4552230
4 250154 250154 4234280 4234280 180126 180126 3976680 3976680
5 289161 289161 4372220 4372220 212137 212137 4481720 4481720
6 142585 142585 4205400 4205400 162688 162688 3638700 3638700
7 205058 205058 3704710 3704710 232817 232817 4972690 4972690
8 128737 128737 3923190 3923190 258483 258483 4435460 4435460
9 214889 214889 4387180 4387180 206285 206285 4515790 4515790
10 216653 216653 4709280 4709280 192290 192290 3918360 3918360
11 148920 148920 4164040 4164040 176967 176967 3875540 3875540
12 190117 190117 4074990 4074990 219689 219689 3990610 3990610
13 205378 205378 3551440 3551440 227852 227852 4256840 4256840
14 185926 185926 4240490 4240490 191623 191623 4801090 4801090
15 100990 100990 4630530 4630530 300162 300162 3838930 3838930
16 230022 230022 4223670 4223670 118266 118266 3049710 3049710
17 158248 158248 3650040 3650040 258493 258493 4078930 4078930
18 180562 180562 5656020 5656020 209388 209388 3931060 3931060
19 221737 221737 4071180 4071180 271833 271833 4483570 4483570
20 123025 123025 3930380 3930380 252484 252484 3786650 3786650
21 307689 307689 3925950 3925950 197840 197840 3518510 3518510
22 130446 130446 3658620 3658620 90032.4 90032.4 3780920 3780920
23 216960 216960 3854220 3854220 170303 170303 3510470 3510470
24 136024 136024 4349670 4349670 242080 242080 3427490 3427490
25 182458 182458 3826970 3826970 99586 99586 3503370 3503370

The parameters are identical from run 1 and run2. If that’s acceptable … then no problem.

Here is a simple fix. If I add the directive: “.options SEEDCLOCK” I do truly get randomized parameters from run to run.

Here’s a partial output captured of the “random” avol1, gbw1, avol2, and gbw2 parameters for the 1st run and the 2nd run with the .options SEEDCLOCK.

step avol1 (run 1) avol1 (run 2) gbw1 (run 1) gbw1 (run 2) avol2 (run 1) avol2 (run 2) gbw2 (run 1) gbw2 (run 2)
0 200000 200000 4000000 4000000 200000 200000 4000000 4000000
1 99066.8 230094 3973200 3710650 242487 142531 4368830 3656140
2 223299 178573 4452570 3992130 237386 170344 3856210 4495030
3 129566 219867 5436200 3378150 140847 174626 3102280 4526370
4 214823 289782 3764360 3685790 162889 189028 3901220 3896050
5 184928 212195 4450730 4137070 175628 161147 3675290 3706210
6 171717 215465 3632320 4307740 171884 126965 4457690 3825770
7 198111 196409 3127750 3954230 213419 169771 3340970 4904060
8 113898 179195 4713340 4363560 176614 189311 3669130 4271810
9 216053 197067 3765520 3669200 219271 190560 4591550 3936160
10 201309 191408 3770870 3892060 181966 79162.8 3822660 3836830
11 151593 132399 3062680 4088730 222056 60681.1 4735460 4326080
12 173595 193581 4003760 3722160 234267 118851 4679570 3554630
13 149505 226978 4121920 4265440 160019 285073 4119580 3865630
14 238609 225370 3089840 4323420 199878 231502 4729170 4290200
15 183963 182607 4874090 4336910 255134 141937 4727710 3851280
16 224755 227259 3933120 4061540 300328 215687 4308960 4886290
17 174336 261532 3984640 3643840 207702 195073 4259050 3477780
18 121901 283052 3641390 4675190 217868 122845 4759560 4326220
19 209471 169820 4155790 3633970 164764 214039 4272270 3351830
20 82690.9 231901 4250400 4607530 137171 248795 3667120 3697340
21 163748 246549 4472870 3694210 210166 187182 3869980 4564510
22 181650 244758 3422330 4013800 268216 192473 3753430 4240000
23 246938 133963 3695040 4368690 192687 368281 3359270 4526340
24 194017 246861 4723870 4193620 260575 137192 4171140 3414740
25 211399 267894 4271580 4793780 233851 179067 3311060 3816940

It can be clearly seen that the parameters from run-to-run are different.

The exception in both cases is the first step (0). This is intentional by the designer to provide the nominal values of avol1(=200K), gbw1(=4Meg), avol2(=200K), and gbw2(=4Meg) as a reference.

Issue #2
I’m currently gathering more data. Will publish in a later posting.

Len

This is not an issue but the nature of random generation by computer. Computer-generated random numbers are typically Pseudo-Random Number Generators. The random number is generated from a seed, and users can assign a seed with .option SEED=<value>. With the same seed, the random pattern is exactly the same in each execution.

To generate different random pattern in each execution, .option SEEDCLOCK can be used to utilize the system clock as the seed, ensuring that in each execution, the seed is different. This is essentially how random numbers behave in computer programming.

You pointed out an important aspect that the random pattern generated in the functions gauss() or random() only generates random numbers in its execution, but this result stays the same in every execution unless include .option SEEDCLOCK. I am only trying to explain that this is not an “issue” but rather a characteristic in random number generation. Issue typically implies a problem or something that needs to be addressed or fixed?

1 Like

@KSKelvin ,

I understand your statements. This is how the “random” functions may work without a random seed.

My concern is that in the Monte Carlo sim being presented, only 100 iterations are used. Therefore, without introducing .option SEEDCLOCK, all the results will be repeatable. Fine if this is the desire of the user. It does seem to fly in the face of what random functions are intended for. The consistency of randomness should be in the distribution of the curve (ie gaussian, linear, etc).

Issue #1 is a “potential” issue that I was alerting a user. If this is the desired effect, then the data will be repeatable.

Len

Issue #2

Here is an issue for me that I originally found in another sim. This issue can appear in the Monte Carlo stepped sim as well.

When assigning random value in .param in a non-stepped sim, the value remains the same value for the entire sim across ALL instances of my use of this in different components or directives in the circuit. This is as expected.

However, if I run this same sim as a stepped sim, EACH instance of the use of “varname” has a NEW random value! This is unexpected and, in my case, causes significant problems with obtaining accurate results.

Here is a simple reduced sim schematic to illustrate:
Random_Issue.qsch (2.3 KB)

If I uncomment “.param run 2” and comment “.step param run 1 2 1”, I run the sim as non-stepped.

.DISPLAY AVOL_1= 172148.206739857 AVOL_2= 172148.206739857
.meas rlts1 find v(avol_1) at time=0:
172148 0.1
.meas rlts2 find v(avol_2) at time=0:
172148 0.1
In all 4 cases where avol was used (2 .display args and 2 B-source args), the single random value of 172148 is used.

I uncomment “.step param run 1 2 1” and comment “.param run 2”.

1 of 2 steps: .step run=1
.DISPLAY AVOL_1= 200000 AVOL_2= 200000
2 of 2 steps: .step run=2
.DISPLAY AVOL_1= 113615.304178692 AVOL_2= 175097.532498391
0 200000 0.1
1 167005 0.1
.meas rlts2 find v(avol_2) at time=0:
0 200000 0.1
1 123198 0.1
Only step 0 is the same non-random value (as per the .func GC(run=0))
The second step (step 1) has 4 different random values (113615…, 175097…, 167005…, 123198…).

In my opinion, this inconsistency in stepped sims can lead to unreliable data.

It is my opinion that once a parameter is calculated before time executing the sim, it remains the same. This is evident when my example sim is non-stepped. Same value throughout.

I used the .display directive to verify the “varname” value. To my surprise, it was “varname” was different in multi-stepped sims!

Applying this logic to the Monte Carlo sim in this thread: Imagine if the user wanted to use the same avol1 and gbw1 across both Amps in the 100 step sim. You couldn’t guarantee the same random value for each parameter.

Len

Don’t use .display to return a randomly generated parameter! I reported the use of .display to return a random value to Mike before. This is Mike’s reply. This is possibly one of the few situations where we don’t expect to have a solution.

Random() is going to return a different number every time it’s evaluated. The single quotes invoke an evaluation. I don’t know if I can reliably change that.

@KSKelvin ,

Interesting. So then, when a .param is called it is re-evaluated each time it’s used.

What explains my non-stepped use of it? In the non-stepped case, the random value parameter remains the same even though I called it 4 times.

Len