have you ever tried to access Channel Impulse Response data from accumulator? I can not retreive it. Right after getting frame receive interrupt I call 20 bytes of ACC_MEM_ID register, and I get only 0x00 byte values. Receiver clocks are on (RXCLKS in PMSC_CTRL0). Can any other settings/bits have an impact on that matter? Have you ever successfully read ACC_MEM register values? I do not use Decawave software, so there is possibility I dont set up the chip properly.
Any suggestions?
Yes, I am loading LDE code. Basically, I can perform full ranging sequence with multiple anchors. It may be, that despite some wrong settings my application is working but I just dont have an access to CIR data. Any other suggestions?
I have solved my issue. I was not enabling AMCE bit in PMSC register. To be clear, to retreive accumulator data you have to set RXCLKS to 01 and set FACE and AMCE bits
I think we met the similar problem. Can you explain a little more about
" I was not enabling AMCE bit in PMSC register. To be clear, to retreive accumulator data you have to set RXCLKS to 01 and set FACE and AMCE bits :)" ?
Codes would be more helpful. Thanks.
unfortunately, I am not able to share my code due to copyrights. Which part of “…you have to set RXCLKS to 01 and set FACE and AMCE bits” you don’t understand?
As far as I remember, those birs are responsible for clocking of the accumulator access bus.
Thanks for sharing your experience on accessing accumulator data. By following your steps, I am able to readback non-zero values. However, the value does not look plausible because there are many spikes within the entire range of 0~1016, either real or imaginary part, which means magnitude of channel impulse response is always large. I tested in indoor LOS. Do you see this before?
Encountered this before. Just a quick note: the 16-bit data in ACC_MEM is stored as signed integer with a range of [-32768, 32767]. See if this resolves your issue.