Which channel model does the DW1000 use, and is there any relevant information?Is the chip receiving the signal of the first arrival path or the strength path?
Hi Lei_Ding,
DW1000 chip can able to receive the signal of First Path.
For More details - Please refer the section 4.7(Assessing the quality of reception and the RX timestamp) in DW1000 User Manual.
Thanks & Regards,
Deepa
Hi Deepa,
When I finished reading the 4.7 section, I found that the DW1000 chip did not process the signal of the first path as the final positioning signal. How does the DW1000 determine which path signal should be received?