Will the dimension of the magnitude along the Y axis be obtained with a low-signal analysis of AC, for example 2A or 10V, as it is done in LTspice?
Maybe there is some way to manually add a dimension to the axis? This could be useful for publishing or reviewing screenshots that are out of context.
Yes, you can. You need to multiply by 1A or 1V or 1W, depending on what you need.
1 Like