i would like to know where the Tag limit comes from.
I read the system overview document. I read in previous topics that it has to do with the superframe.
I understand that a superframe has 15 slots, and a superframe can be sent every 100ms.
So i get that 60 (seconds in a minute) * 0.1 seconds (length of superframe) * 15 (slots in superframe) = 9000. Which is the maximum number of tags in a minute. But i do not understand why this method cant continue after 60 seconds.
Hi,
are 16 slots.
I think that, for example:
if you has 5000 tags without moving, in the minimal update frequency(0.016)
5000*0.016=80Hz
150-80=70Hz
You can has 70 tags moving, updated in each second(1Hz), or 35 updated in each 0.5 (2Hz).