40Watt output SSPA Ka Band

Hello,
I will be designing an SSPA with a 40-watt output operating between 27 and 31 GHz for my thesis. I am considering using the QPA2212T MMIC as a final power stage. Is this product suitable for this purpose, and if so, which component can I use as a driver to operate it? Could you give me some advice on this? Thank you.

Yes you could use the QPA2212T. It may be slightly short on power when you take into account the combining loss, assuming you combine 2 MMICs to reach 40W. TGA4509 could be used as a driver.

I was considering using the QPA2210D as a driver. Is this component suitable? Is the TGA4509 a better option?

The QPA2210D is no longer available. It is too high in power to use as a driver for 2*QPA2212T. The QPA2212T only needs around 25dBm input power. TGA4509 as driver is a good option.

Thank you for your replies,
But Qorvo webpage for the TGA4509 states: “End of Life announced June 19, 2015. Last Time Buy April 7, 2016.” I am not sure if this product is still in production and available. Could it be an old, discontinued product?
https://www.qorvo.com/products/p/TGA4509

That’s an error on the new web-site. Apologies for this. The TGA4509 is still in full production.

Is the TGA2594 suitable, then? It appears more advantageous in terms of gain, and it is also listed as an alternative to the QPA2210D on the Qorvo website.

TGA2594 is no longer available. It went end of life in 2023.