Having a set of DWM1001-DEV lying around here, I would like to build a “semi-tracking” system with the following features:
- 2 fixed anchors, 1 is connected to a host PC
- multiple moving tags
- the connected anchor should be able to give me the following distances: anchor1-tag(s), anchor2-tag(s), anchor1-anchor2
I don’t want to use the tracking engine, but only individual ranging in the above manner. Is this possible with the included firmware? From what I can see in the documents it is possible to do a simple ranging between 1 tag and 1 anchor (one being connected to host), but in my case I need an additional “remote ranging” between the second anchor and the tag.
I would appreciate any idea!