// Automatically generated C++ file on Sun Jul 21 10:04:20 2024 // // To build with Digital Mars C++ Compiler: // // dmc -mn -WD comp_edget.cpp kernel32.lib #include extern "C" __declspec(dllexport) int (*Display)(const char *format, ...) = 0; // works like printf() extern "C" __declspec(dllexport) const double *DegreesC = 0; // pointer to current circuit temperature union uData { bool b; char c; unsigned char uc; short s; unsigned short us; int i; unsigned int ui; float f; double d; long long int i64; unsigned long long int ui64; char *str; unsigned char *bytes; }; // int DllMain() must exist and return 1 for a process to load the .DLL // See https://docs.microsoft.com/en-us/windows/win32/dlls/dllmain for more information. int __stdcall DllMain(void *module, unsigned int reason, void *reserved) { return 1; } void bzero(void *ptr, unsigned int count) { unsigned char *first = (unsigned char *) ptr; unsigned char *last = first + count; while(first < last) *first++ = '\0'; } // #undef pin names lest they collide with names in any header file(s) you might include. #undef in1 #undef in2 #undef Q #undef riseT #undef fallT struct sCOMP_EDGET { // declare the structure here double lastQ; }; extern "C" __declspec(dllexport) void comp_edget(struct sCOMP_EDGET **opaque, double t, union uData *data) { double in1 = data[0].d; // input double in2 = data[1].d; // input bool &Q = data[2].b; // output double &riseT = data[3].d; // output double &fallT = data[4].d; // output if(!*opaque) { *opaque = (struct sCOMP_EDGET *) malloc(sizeof(struct sCOMP_EDGET)); bzero(*opaque, sizeof(struct sCOMP_EDGET)); } struct sCOMP_EDGET *inst = *opaque; // Implement module evaluation code here: // compare input, >= set output is same characteristic of Qspice SCHMITT if (in1 >= in2) Q = 1; else Q = 0; // assign current time (t) at rising or falling edge if (Q && !inst->lastQ) riseT = t; if (!Q && inst->lastQ) fallT = t; inst->lastQ = Q; } extern "C" __declspec(dllexport) double MaxExtStepSize(struct sCOMP_EDGET *inst) { return 1e308; // implement a good choice of max timestep size that depends on struct sCOMP_EDGET } extern "C" __declspec(dllexport) void Trunc(struct sCOMP_EDGET *inst, double t, union uData *data, double *timestep) { // limit the timestep to a tolerance if the circuit causes a change in struct sCOMP_EDGET const double ttol = 1e-9; if(*timestep > ttol) { bool &Q = data[2].b; // output double &riseT = data[3].d; // output double &fallT = data[4].d; // output // Save output vector const bool _Q = Q ; const double _riseT = riseT; const double _fallT = fallT; struct sCOMP_EDGET tmp = *inst; comp_edget(&(&tmp), t, data); // if(tmp != *inst) // implement a meaningful way to detect if the state has changed // *timestep = ttol; if(tmp.lastQ != inst->lastQ) *timestep = ttol; // Restore output vector Q = _Q ; riseT = _riseT; fallT = _fallT; } } extern "C" __declspec(dllexport) void Destroy(struct sCOMP_EDGET *inst) { free(inst); }