/** * LEAPS - Low Energy Accurate Positioning System. * * Simple user application. * * Copyright (c) 2016-2017, LEAPS. All rights reserved. * */ #include "dwm.h" #include #define SLEEP_BTN_GPIO DWM_GPIO_IDX_2 #define LED_BTN_GPIO DWM_GPIO_IDX_14 #define SLEEP_BTN_CHECK_PERIOD_TICKS 2 /* Thread priority */ #ifndef THREAD_APP_PRIO #define THREAD_APP_PRIO 20 #endif /* THREAD_APP_PRIO */ /* Thread stack size */ #ifndef THREAD_APP_STACK_SIZE #define THREAD_APP_STACK_SIZE (3 * 1024) #endif /* THREAD_APP_STACK_SIZE */ #define APP_ERR_CHECK(err_code) \ do { \ if ((err_code) != DWM_OK) \ printf("err: line(%u) code(%u)", __LINE__, (err_code));\ } while (0) \ #define MSG_INIT \ "\n\n" \ "App : dwm-simple\n" \ "Built : " __DATE__ " " __TIME__ "\n" \ "\n" /** * Event callback * * @param[in] p_evt Pointer to event structure * @param[in] p_data Pointer to user data */ void CheckButton(void) { bool value; int res; // #define DWM_OK (0) res = dwm_gpio_value_get( SLEEP_BTN_GPIO, &value); //printf("VALOR DE RES > %d \n",res); //printf("VALOR DE VALUE > %u \n", value); //if ( res != DWM_OK ) { //res = dwm_gpio_value_set( LED_BTN_GPIO, 0); //printf("DWM OK \n"); // in case of any error assuming button is not pressed //return false; //} // check pin value, light LED if pressed and return current button state if ( value == 0 ) { dwm_gpio_value_set( DWM_GPIO_IDX_14, true); res = dwm_gpio_value_set( LED_BTN_GPIO, 0); printf("LED APAGADO\n"); //return true; }else{ dwm_gpio_value_set( DWM_GPIO_IDX_14, false); res = dwm_gpio_value_set( LED_BTN_GPIO, 1); printf("LED PRENDIDO\n"); //return false; } } void on_dwm_evt(dwm_evt_t *p_evt, void *p_data) { int i; switch (p_evt->header.id) { /* New location data */ case DWM_EVT_NEW_LOC_DATA: /* Process the data */ printf("\nT:%lu ", dwm_systime_us_get()); if (p_evt->data.loc.p_pos == 0) { /* Location engine is disabled */ } else { printf("POS:[%ld,%ld,%ld,%u] ", p_evt->data.loc.p_pos->x, p_evt->data.loc.p_pos->y, p_evt->data.loc.p_pos->z, p_evt->data.loc.p_pos->qf); } for (i = 0; i < p_evt->data.loc.anchors.dist.cnt; ++i) { printf("DIST%d:", i); printf("0x%04X", (unsigned int)(p_evt->data.loc.anchors.dist.addr[i] & 0xffff)); if (i < p_evt->data.loc.anchors.an_pos.cnt) { printf("[%ld,%ld,%ld]", p_evt->data.loc.anchors.an_pos.pos[i].x, p_evt->data.loc.anchors.an_pos.pos[i].y, p_evt->data.loc.anchors.an_pos.pos[i].z); } printf("=[%lu,%u] ", p_evt->data.loc.anchors.dist.dist[i], p_evt->data.loc.anchors.dist.qf[i]); } printf("\n"); break; default: break; } /* Indicate the application has finished the tasks and can now */ dwm_sleep(); } /** * Application thread * * @param[in] data Pointer to user data */ void app_thread_entry(uint32_t data) { dwm_cfg_tag_t cfg_tag; dwm_cfg_t cfg; uint8_t i2cbyte; int rv,RESPUESTA; RESPUESTA = dwm_gpio_cfg_input( SLEEP_BTN_GPIO, DWM_GPIO_PIN_PULLUP); // configure LED pin, blink twice dwm_gpio_cfg_output( DWM_GPIO_IDX_14, false); /* Initial message */ printf(MSG_INIT); /* Get node configuration */ APP_ERR_CHECK(dwm_cfg_get(&cfg)); if ((cfg.mode != DWM_MODE_TAG) || (cfg.accel_en != false) || (cfg.loc_engine_en != true) || (cfg.meas_mode != DWM_MEAS_MODE_TWR) || (cfg.low_power_en != false) || (cfg.common.fw_update_en != false) || (cfg.common.uwb_mode != DWM_UWB_MODE_ACTIVE) || (cfg.common.ble_en != true) || (cfg.common.led_en != true)) { /* Configure device as TAG */ cfg_tag.accel_en = false; cfg_tag.loc_engine_en = true; cfg_tag.low_power_en = false; cfg_tag.meas_mode = DWM_MEAS_MODE_TWR; cfg_tag.common.fw_update_en = false; cfg_tag.common.uwb_mode = DWM_UWB_MODE_ACTIVE; cfg_tag.common.ble_en = true; cfg_tag.common.led_en = true; APP_ERR_CHECK(dwm_cfg_tag_set(&cfg_tag)); dwm_reset(); } /* Update rate set to 1 second, stationary update rate set to 5 seconds */ APP_ERR_CHECK(dwm_upd_rate_set(10, 50)); /* Register event callback */ dwm_evt_cb_register(on_dwm_evt, 0); /* Test the accelerometer */ i2cbyte = 0x0f; rv = dwm_i2c_write(0x33 >> 1, &i2cbyte, 1, true); if (rv == DWM_OK) { rv = dwm_i2c_read(0x33 >> 1, &i2cbyte, 1); if (rv == DWM_OK) { printf("Accelerometer chip ID: %u\n", i2cbyte); } else { printf("i2c: read failed (%d)\n", rv); } } else { printf("i2c: write failed (%d)\n", rv); } while (1) { /* Thread loop */ CheckButton() ; // delay 20ms dwm_thread_delay(20); } } /** * Application entry point. Initialize application thread. * * @warning ONLY ENABLING OF LOCATION ENGINE OR BLE AND CREATION AND STARTING OF * USER THREADS CAN BE DONE IN THIS FUNCTION */ void dwm_user_start(void) { uint8_t hndl; int rv; dwm_shell_compile(); dwm_ble_compile(); dwm_le_compile(); dwm_serial_compile(); /* Create thread */ rv = dwm_thread_create(THREAD_APP_PRIO, app_thread_entry, (void*)NULL, "app", THREAD_APP_STACK_SIZE, &hndl); APP_ERR_CHECK(rv); /* Start the thread */ dwm_thread_resume(hndl); }