We have 10-20 devices on the same channel but they are running on 6M8, on 110k I have only two devices which I’m testing it on. (I tried testing on other channels)
I see the issue with preambles 1536 and up. I’m using mainly 2046. I can provide values of whole register map or log communication over SPI, would that help?
We use ACK only for testing purposes so we solved it by adding manual RX turn off and on. It’s not something important to get working now so If you don’t have any other input we can close it.
Another information about PAC: When using PAC32 it doesn’t fix that problem but DW never gets stuck forever, it’s RX dies for few seconds and then start’s receiving again. It’s only when I’m using PAC64 that DW RX get’s stuck permanently. I will take a closer look at that next week.