Hi,
I have a micro controller attached to DWM1001. I checked connection is working ok with several “get” commands.
Is there a specific sequence to use for setting up a device as an anchor?
I sent a setup command 0x07, 0x02, 0x9e, 0x00 and received correct response 0x40 0x01 0x00.
The I did a dwmcfg_get and received 0x40 0x01 0x00 0x02 0x1e 0x30
However, now every time I try to change the setting (I want to disable BLE) I keep getting an error back → 0x40 0x01 0x01 (unknown command), even though it is the same commend I used successfully initially.
The odd thing is that all the read/get commands work fine and return the correct values. Any set command results in error 0x01.