I use the example firmware 5(a) and 5(b) and another EVK1000 in listen mode to monitor the messages between the Initiator and Responder.
The issue on the Responder:
When this line is executed - [color=#3399ff]ret = dwt_starttx(DWT_START_TX_DELAYED | DWT_RESPONSE_EXPECTED); [/color]the response message is only transmitted after about 16 Seconds, it appears Tx happens when the counter rollover. Even if I change [color=#3399ff]#define POLL_RX_TO_RESP_TX_DLY_UUS 2600 [/color] To another value; Tx only happens after about 16 Seconds.
With [color=#3399ff]POLL_RX_TO_RESP_TX_DLY_UUS 2600[/color] it appears that the resp_tx_time is set correctly
[color=#3399cc]poll_rx_ts 48FC18EA7B[/color]
[color=#3399cc]resp_tx_time 490640EA[/color]
I also monitor [color=#3399ff]if (ret == DWT_ERROR) [/color]and [color=#3399ff]HPDWARN[/color], none is set!
Thank you in advance
Andre