Guys:
I need to create the topology shown in the figure attached. There are 12 anchors, 3 gateways, one initiator.
I assumed that all anchors are in range of gateways. I will use dwm-1000 dev kit with default configurarion , which is 6.8Mbps. This topology is intended to be installed in an open area.
I did a test with one square with 4 anchors and 1 GW with the same dimensions and worked fine.
The point is:
- One initiator is enough or should I put more initiators as some anchors are far from A1 (initiator)
- If one tag is in range of two simultaneous gateways, will both receive the same data ? Then when I save in the database I shall remove duplicity?
- Is there any problem with an anchor which has coverage from two different gateways (for instance A2, GW1 and GW2)
- What are the chances that this topology work ? Shall I put one more gateways (GW4, let’s say) inside the 3rd square on top ?
I’d appreciate any help as soon as possible.
Regards
Andre