This Portion of code is extracted from the Deca-Driver inside of the source code of the DWM1004C TDoA Tag Firmware
#define TEMP_COMP_FACTOR_CH2 (327) //(INT) (0.0798 * 4096)
#define TEMP_COMP_FACTOR_CH5 (639) //(INT) (0.156 * 4096)
From where them come the 327 and 639 values for channel 2 and 5 respectively,
What is the purpose of these values?
how can I get these values for channel 1,3,4 and 7?
or anybody has the values for the remaining channels?
What happen if I leave these values as 0?
What I’m trying to do is to modify the code to enable the remaining channels 1,3,4 and 7.