Hi,
I’m syncronizing more anchors with external clock and external sync procedure. As reported in the last point of the “Synchronization process” in the application note APS007 ( WIRED SYNCHRONIZATION OF ANCHOR NODES IN A TDOA REAL TIME LOCATION SYSTEM ) : “The micro-controller in each anchor node receives an interrupt from the DW1000 indicating that the OSTR has occurred” .
I’m tryng to catch this interrupt but I don’t see any interrupt after the sync signal is sent and received from dw1000. This interrupt is really generated from dw1000? If yes, how can I anable it?
Thanks