[size=large][font=Arial]Hello,
[/font][/size]
[size=large][font=Arial] Using DWM1001 modle.
[/font][/size]
[size=large][font=Arial] I have some problems and I hope to ask you.[/font][/size]
[size=large][font=Arial] The area is 52m*18m with 88 [size=large][font=Arial]DW1001[/font][/size] modle. There is a [size=large][font=Arial][size=large][font=Arial][size=large][font=Arial]corridors[/font][/size][/font][/size][/font][/size] in the middle. There are about 20 rooms on both sides, 3 dw1001 are placed in each room, and several dw1001 are placed in the corridors. [/font][/size]
[size=large][font=Arial] Firstly, when the room door is opened, the anchors in the [size=large][font=Arial][size=large][font=Arial]corridors[/font][/size][/font] [/size]and the [size=large][font=Arial]anchors[/font] int the[/size] room can be normally connected, but one initiator just only connect 16 [size=large][font=Arial][size=large][font=Arial]anchors[/font][/size][/font][/size]. If multiple initiators are set up, some [size=large][font=Arial][size=large][font=Arial]anchors[/font] [/size][/font][/size]cannot get data. [/font][/size]
[size=large][font=Arial] Secondly, if the [size=large][font=Arial]room[/font] [/size]door is closed, [size=large][font=Arial]the anchors[/font] in[/size] the room cannot be connected to [size=large][font=Arial]initiators [/font]in outside[/size]. [/font][/size]
[size=large][font=Arial] Thirdly,sometimes,[size=large][font=Arial][size=large][font=Arial] tag’s[/font] pos message[/size][/font][/size] is “POS,0,0000,0,0,0,0,0”,why?([size=large][font=Arial]get date[/font] by [/size]passive)[/font][/size]
[size=large][font=Arial] At last,Is tag included in the limit of the max (16) seats?[/font][/size]
[size=large][font=Arial]The following is a screenshot of the area. What steps can be taken to solve these two problems?[/font][/size]