Hi…
I have a raspberry Pi Zero W attached to a DWM1001. They are attached via header pins 2, 4, 6, 8 & 10 so that I can send serial commands from the Pi to the DWM1001.
I am trying to send serial shell API commands to the DWM1001. It seems as though I can only send a max of about 6 characters. Any commands less than this seem to work fine. I get a full response without and truncation. But commands longer than 6 won’t go though.
ex…
echo -e “si\r” > /dev/serial0
This works as only 3 chars are required…
this get truncated…
echo -e “aps 12 34 56\r” > /dev/serial0
Only the “aps 12” gets through.
I thought maybe it was a buffer size issue or even the miniuart. I switched off the blue tooth and swapped the miniuart with the good one but it didn’t seem to make much difference.
-Console is disable via cmdline.txt
-uart is enabled via config.txt
-bt is off via config.txt
-hciuart service is disabled
If anyone has any idea why I am getting this truncation I would really appreciate the help.
Thanks,
Pat