Seeking Example Code for UWB and Bluetooth Operation on QM33120WDK1

Hello Qorvo Community,

I’m working with the QM33120WDK1 development kit which features both UWB and Bluetooth 5.3 capabilities. While the SDK includes separate example projects for UWB and Bluetooth functionality, I’ve been unable to find or create a working example that implements both technologies simultaneously.

I’ve been working with the following example projects from the SDK:

  1. UWB Example:
    DW3_QM33_SDK_1.0.2/Drivers/API/Build_Platforms/nRF52840-DK/dw3000_api.emProject

  2. Bluetooth Example:

DW3_QM33_SDK_1.0.2/Drivers/API/Build_Platforms/nRF52840-DK/sdk/examples/ble_peripheral/ble_app_blinky/pca10056/s140/ses/ble_app_blinky_pca10056_s140.emProject

Questions:

  1. Are there any example solutions in the SDK that demonstrate simultaneous UWB and Bluetooth operation?
  2. If not, could someone provide guidance on how to combine these functionalities?

Thank you in advance for your help!

~Pavel

Download the QNI code for DWM3001CDK. It would give you a great starting point, because that is a complete bundle.