Hello guys, I have a question related to the antenna radio pattern of dwm1001 device.
I already know that those antennas are vertically polarized, means that they obtain the “almost” omnidirectional pattern if vertically placed.
I installed a tripod on the ground and put on it an antenna which is more or less at 1 meter above the ground.
Now I have a drone that flies on the sky at altitude 10 meters.
I placed another antenna on the drone, vertically, but in a reverse way, since I thought that the uwb transceiver should have been positioned in such a way to have as much as possible free space.
Not consider that the antenna on the ground is positioned at the origin (0, 0) and that the drone start to fly on the sky at a fixed speed of 5 m/s. The drone continuously sends its actual GPS coordinates taken from its installed GPS module.
In order to do that, the drone converts the GPS coordinates into local (x, y) coordinates relatively to the origin (0, 0).
The antenna on the ground has the leds that look the “south” where the leds on the antenna on the ground look the “north” pole.
Just to better understand the meaning of north and south, north is towards a positive y-coordinate, south the opposite.
The drone starts from (-30, -100) and goes to (-30, +100), hence it runs “bottom-up”.
Checking the log, I saw that the drone “refreshes” its new local (x, y) position every 0.6-0.7 meters in average.
In the other side, the antenna on the ground registers the messages sent by the “drone”. If the sensor hears, for example, (30.45, 76.89), it “casts” the messages in (30, 76). In other words, I’m working on only integer values.
Every time that a sensor hears the same local position, it increases a variable (starting from 0).
However, I attached a plot that represent the messages hear by the antenna on the tripod.
In this figure, three scan have been reported, where a “scan” is simply a vertical line followed by the drone “bottom-up”.
The first scan is in -30, the second in 0, and the third in +30.
The strange thing is that the heard “line” on the left is different from the one heard at +30.
Why? I was expecting to have almost the same behavior.
Moreover, this occur always: repeating the experiment, changing the place, setting different speeds and altitudes…
Thanks.