I would like to simulate the LED with input voltage 5V. How to define the R_ser to achieve VF 3V since there is no information about the R internal of LED? Based on the forward voltage vs forward current, I think the internal resistor is depend on the forward voltage. For the example at VF 3V, R_int = 3/0.15 = 20 Ohm, then for my input 5V I should connect the R_ser = 13.3 Ohm. Please review my analysis and looking for your feedback all. Thank you.
example_led.qsch (2.2 KB)