Quick Deployment Guide

I’ve been going through Decawaves quick deployment guide with the ultimate objective of connecting a DWM1001 via a Pi. It’s been an accurate and good guide thus far but I’ve run into a speed bump at section 4.4 Gateway Configuration. I type the command ls -1 /etc/dwm1001
and then see several configuration scripts displayed, so far so good. When I type in the command sudo vi /etc/dwm1001/dwm1001.conf a blank vi file opens instead of an existing one. Is this correct?

Capture01 Capture02

1 Like

I have the same problem

The problem is in the datasheet it says to type “sudo nano /etc/dwm1001/dwm1001.conf”. However, the last part should be “.config” instead of “.conf”

Hi, could you please leave here the link of that “quick deployment guide”. Thank you.

Hi @electronic_user_1
here is the link DWM1001 Gateway Quick Deployment Guide - Decawave

Cheers
JK