Hi Qorvo team,
We’re using the DWM3001CDK dev board with QANI firmware v1.1.1 for Nearby Interaction with iPhones. We’re seeing compatibility issues across different iPhone models:
| iPhone Model | Chip | Result |
|---|---|---|
| iPhone 11 | U1 | Works perfectly, 5Hz stable |
| iPhone 12 Pro Max | U1 | Fails immediately after BLE connection, UWB session never starts |
| iPhone 15 | U2 | Only the first ranging frame succeeds, subsequent frames all return raw_status=33 (RX timeout) |
We confirmed:
- The Accessory Configuration Data (ACD) is identical across all connections
- 1Hz mode works on iPhone 15, only 5Hz (User Interactive) fails
- The block timing is stable at ~162ms on the accessory side
Is this a known issue? Is there an updated QANI firmware that supports newer iPhone models and iOS versions?
Thanks,