Probing and waveform viewer

@LucasDB Oh, I review Olli message again and definitely my mis-understanding. ALT only solve probing without moving wire or device but not vice versus. Thanks for reminding me.
I personally not ran into this problem frequently as I highly rely on using .plot command and close waveform viewer before simulation is run and regenerate plot as according to .plot if I changed something. But I understand your concern about moving wire/device mess the waveform viewer or scaling issue.

Let wait and see if waveform viewer will evolve in future. Possibly waveform viewer is not as essential as simulator during this beta phase, and bug fixing is priority. I believe it will eventually get improve after Mike collects more feedback from different users and come up with the best. You know, different people have different opinion what the best implementation.

At this point, I also need to write program to handle plot or thing that waveform viewer currently not support. Have to be in patient as may be many priority items are on the list.

1 Like

I totally agree with LucasDB:
these two items should be fixed.
It seems we need two knobs:

  1. to switch off autoscaling
  2. to switch off probing (while editing schematics)
3 Likes

@paulQ

I totally agree with LucasDB:
these two items should be fixed.
It seems we need two knobs:

  1. to switch off autoscaling
  2. to switch off probing (while editing schematics)

You have my vote :+1:

I would be Ok with never being in “probe mode” unless you held down some key or combo.

I use the plot window save function to “avoid” auto scale but it sure would be great if you could “save” the plot window settings and re-run the sim and the plot would not just jump back to auto scale mode, that is super annoying.

Mike has recently implemented a new feature that allows to suspend cross-probing between the schematic and the waveform viewer. You may have noticed this update, but it does not specify where to find this option. After confirming with Mike, here is how you can enable or disable this feature: The option will only appear if there is an active waveform viewer window that is cross-probing to the schematic.

06/17/2024 Implemented the ability to suspend cross probing off so you can edit a schematic without changing the waveform setup.

Hi Kelvin, this morning (at me at least) after update also some new features appears meanwhile, apart from Suspend cross probing. Add also these to the documentation.
image

2 Likes

That is great! However, still not as easy to use as LTspice as you have to constantly go into that menu to suspend and activate cross probing when you make some changes to the circuit and don’t want the waveforms to be messed up. Some kind of keyboard shortcut is needed. Ideally, I would like it to behave so that cross probing could be suspended by default and activated momentarily by pressing and holding a keyboard key (eg. Alt).

I agree that accidentally messing up the plot window is a nuisance. But I am still getting used to Qspice…

I open and update QSPICE every now and then to see if there are any updates made to the QUI. Now I noticed that there is a keyboard shortcut (P) implemented for “Suspend cross probing”. It’s a good but very small improvement. Still, I hate that cross probing is on by default and you can’t start moving things after a simulation run without remembering to suspend cross probing. I think the user should have the option to set editing the schematic as a default operating mode and probe only with pressing and holding a specific key (eg. Alt).

I would love to start using QSPICE but this is so annoying feature that I just can’t.