In order to get around a hardware error on a custom DWM1003 board, I’d like to move the DW_IRQ to GPIO 10 which is also used for NFC2. So I redefined DW1000_IRQ_A_Pin as 10 instead of 19 and added a define for CONFIG_NFCT_PINS_AS_GPIOS to use the NFC pins as GPIO.
Pin 4 of the module (now DW_IRQ) has an interrupt happening but the firmware never enters dwt_isr() when debugging with a breakpoint in this routine.
Is the some other setup I need to do to use the NFC2 pin as theDW_IRQ?
Regards,
Jas