The information is the CIR memory - Register 25 in the DW1000.
The Decawave drivers provide a means to read this. Or if you are writing your own firmware the code below worked for me and should be fairly easy to translate to however you are accessing the device. One warning, this must be done after a packet has been received but before you re-enable the receiver. As soon as you enable receive this memory is wiped. My initial attempt at this failed because my receive interrupt automatically re-enabled things 
void enableCIRMemory(bool enable) {
uint16_t regValue = readRegister16(DW1000_PMSC,DWPMSC_PMSC_CTRL0);
regValue &= 0x7fb3; // clear bits 15, 6, 2 and 3
if (enable) {
regValue |= (1<<6 | 1<<15 | 1<<3);
writeRegister16(DW1000_PMSC,DWPMSC_PMSC_CTRL0, regValue);
}
void readCIRLine(int line, uint8_t data) {
readRegister(DW1000_ACC_MEM, line4,data, 5);
}
void readCIR() {
int16_t real;
int16_t imag;
uint8_t data[5];
enableCIRMemory(true);
for(int i = 0;i<dataPoints;i++) {
readCIRLine(i,data);
real = ((uint16_t)data[2])<<8 | data[1];
imag = ((uint16_t)data[4])<<8 | data[3];
float mag = (float)realreal + (float)imagimag;
mag = sqrt(mag);
pc.printf("%i,%i,%i,%.1f\n", i,real,imag,mag);
}
enableCIRMemory(false);
}
You can also read out the detected leading edge location, peak and detection thresholds used. I’ve sometimes plotted the threshold and detection point onto the CIR plot, it makes for a useful live diagnostics display when you have something odd going on. The code I used to get those values was:
void readLEDData(uint16_t *threshold, uint16_t *location, uint16_t peak,uint16_t noise, uint16_t leadingEdge) {
readRegister(DW1000_LDE_CTRL, 0, (uint8_t)threshold, 2); // register, sub address, result buffer, bytes to read
readRegister(DW1000_LDE_CTRL, 0x1000, (uint8_t)location, 2);
readRegister(DW1000_LDE_CTRL, 0x1002, (uint8_t)peak, 2);
readRegister(DW1000_RX_FQUAL, 0, (uint8_t*)noise, 2);
uint32_t tmp = readRegister32(DW1000_RX_TIME,4); // register, sub address
*leadingEdge = (tmp>>8) & 0xffff;
}