Nice If The Graphs Could Have An Option To Add A Title On The Fly

Hello,

I noticed from working with graphs, that even though the graph window includes the top bar menu options as well as the righ-click on demand menu options, as shown in the attachment, in either menu there is no option to add a graph title on the fly. Can this option be added?

For example, when you right-click, the menu provides the options to:

  1. Add Plot
  2. Add Window

However, there is no option to:
Add Title