New file upload formats enabled: *.cpp, *.h, *.py

I am pleased to announce we have enabled forum uploads for file types .cpp, .h, and .py. You can now share source code!

Edit: code blocks are also now supported. Other formats, like .qsch and .qsym, are in process.

4 Likes

Thank you, Jeff!!!

Looking forward to the other formats.

–robert

Robert, your code samples were one of the drivers for getting this done :slight_smile:

So I was the squeaky wheel? Not sure how I feel about that. :wink:

–robert

You should feel good about that!

I edited my original post too: code blocks are now supported:

While you’re chasing the file format gremlins, it would be nice if I could edit a post that contains images.

If I’m including images in a post, I’m almost certainly writing a longer-than-average post with a larger-than-average chance that I’ll want to fix some mistake or add some information. Doesn’t matter how many times I review before clicking “reply”…

–robert

2 Likes

@RDunn Yes, I totally agree no way to edit image post is a pain (“error 403”)! In answering someone but made a mistake in reply, I prefer can edit the answer instead creating one more post follow the typo one.

I also agree with Robert

I’m looking into it!

3 Likes