Hello,
I am working on Real-time location system using MDEK1001 kit. I am successfully able to do things with the already built firmware image that has come with the board. I am now trying to implement using my newt as given on the decawav website. I am facing some issues, I posted it on the forum as well as Github site but I didn’t get any support yet. I am posting the issue here.
I erased the default flash image using JLink. Now, while loading the bootloader as per gievn guideline on github, it is stuck at point . I have shown here the verbose that I got :
newt load dwm1001_boot -v
Loading bootloader
Load command: E:/Projects/RTLS/nRF/GitCodes/mynewt-dw1000-apps/repos/mynewt-dw1000-core/hw/bsp/dwm1001/dwm1001_download.cmd E:/Projects/RTLS/nRF/GitCodes/mynewt-dw1000-apps/repos/mynewt-dw1000-core/hw/bsp/dwm1001 bin\targets\dwm1001_boot\app\apps\boot\boot
Environment:
- BOOT_LOADER=1
- FEATURES=BASELIBC_PRESENT BOOT_LOADER BSP_NRF52 CONSOLE_UART_BAUD CONSOLE_UART_DEV CONSOLE_UART_FLOW_CONTROL DW1000_DEVICE_0_IRQ DW1000_DEVICE_0_RST DW1000_DEVICE_0_RX_ANT_DLY DW1000_DEVICE_0_SS DW1000_DEVICE_0_TX_ANT_DLY DW1000_DEVICE_BAUDRATE_HIGH DW1000_DEVICE_BAUDRATE_LOW FLASH_MAP_MAX_AREAS HAL_FLASH_VERIFY_BUF_SZ I2C_0_FREQ_KHZ I2C_1_FREQ_KHZ I2C_1_PIN_SCL I2C_1_PIN_SDA MBEDTLS_AES_C MBEDTLS_BASE64_C MBEDTLS_ECP_DP_SECP224R1 MBEDTLS_ENTROPY_C MBEDTLS_PKCS1_V15 MBEDTLS_PKCS1_V21 MCU_DCDC_ENABLED MCU_FLASH_MIN_WRITE_SIZE MCU_NRF52832 MSYS_1_BLOCK_SIZE NFC_PINS_AS_GPIO OS_CPUTIME_FREQ OS_CTX_SW_STACK_GUARD OS_IDLE_TICKLESS_MS_MAX OS_IDLE_TICKLESS_MS_MIN OS_MAIN_STACK_SIZE OS_MAIN_TASK_PRIO OS_SYSVIEW_TRACE_CALLOUT OS_SYSVIEW_TRACE_EVENTQ OS_SYSVIEW_TRACE_MUTEX OS_SYSVIEW_TRACE_SEM QSPI_FLASH_SECTOR_COUNT QSPI_PIN_CS QSPI_PIN_DIO0 QSPI_PIN_DIO1 QSPI_PIN_DIO2 QSPI_PIN_DIO3 QSPI_PIN_SCK SANITY_INTERVAL SPI_0_MASTER_PIN_MISO SPI_0_MASTER_PIN_MOSI SPI_0_MASTER_PIN_SCK TIMER_0 UARTBB_0_PIN_RX UARTBB_0_PIN_TX UART_0_PIN_CTS UART_0_PIN_RTS UART_0_PIN_RX UART_0_PIN_TX UART_1_PIN_CTS UART_1_PIN_RTS WATCHDOG_INTERVAL XTAL_32768
- FLASH_OFFSET=0x0
- IMAGE_SLOT=0
- CORE_PATH=E:/Projects/RTLS/nRF/GitCodes/mynewt-dw1000-apps/repos/apache-mynewt-core
- BSP_PATH=E:/Projects/RTLS/nRF/GitCodes/mynewt-dw1000-apps/repos/mynewt-dw1000-core/hw/bsp/dwm1001
- BIN_BASENAME=bin\targets\dwm1001_boot\app\apps\boot\boot
After this, nothing is happening . How much time does it takes to upload the bootloader?
Hope to hear from you soon.
Thanks & Regards
Asmita